Technical FAQs

Ask a Question

Is a LexCom Performance test kit required for each installation?

The LexCom Performance test kit (product code VDIR580010) is used to verify the installation work and to enable correct configuration of the installation. 

The test kit:
- Allows the 8 links to be tested
- Tests the wiremap (continuity and shorts)
- Tests cable link length adjustments for TV output level
- Powered by LexCom Performance core unit

Whilst the test kit is available to purchase, it is also possible to arrange to loan the kit for a period of 2 weeks free of charge.  Please contact us on 0870 608 8 608 for further details.
Was this helpful?
What can we do to improve the information ?