Technical FAQs

Ask a Question

What is the recommended maximum spacing between fixings when installing 20mm or 25mm conduit?

Conduit is installed using saddles, spacer bar saddles or quick clip fixings.  The recommended maximum spacing between fixings is 1m.  It is advisable to saddle approximately 150mm on either side of a bend.
Was this helpful?
What can we do to improve the information ?