Technical FAQs

Ask a Question

The letter P is flashing on the display of an ATV212

The letter P flashing on the display of the ATV212 indicates that the bus voltage is going over voltage. This could be due to high line voltage or the regenerative effect of the motor breaking or even a combination of both. Adjustments can be made in F305 and F626 for further information please down load the Programming Manual from our web site
Was this helpful?
What can we do to improve the information ?