Technical FAQs

Ask a Question

My ATV212 has a Flashing ‘E’ on the display and I can not get rid of it

 
The flashing ‘E’ on the display indicates that the drive is in Remote mode and the STOP button on the key pad has been pressed. Check that the fault has been cleared and then if F735 is set to 1 (default) press the stop button twice. The flashing E will now disappear.
 
 
Was this helpful?
What can we do to improve the information ?