Technical FAQs

Ask a Question

What is the difference between an LADR1V and LADR1 reversing contactor kit?

The difference is the LADR1V kit has mechanical & electrical interlocking, where the LADR1 has only mechanical interlock.
See below for what the kits comprise off
 
The complete parts will only fit the LC1D09 to D38 contactors with screw terminals
 
LADR1V           complete kit with electrical interlocking
Individual parts within the kit
  • LAD9V2            mechanical interlock with
  • LAD9V1            electrical interlocking
  • LAD9V5            set of parallel power connections for 3 pole contactors
  • LAD9V6            set of reversing power connections for 3 pole contactors
 
 
LADR1             complete kit without electrical interlocking
Individual parts within the kit
  • LAD9V2            mechanical interlock
  • LAD9V5            set of parallel power connections for 3 pole contactors
  • LAD9V6            set of reversing power connections for 3 pole contactors
Was this helpful?
What can we do to improve the information ?