Technical FAQs

Ask a Question

Will Vijeo Designer work on Windows 7 64 bit?

Yes if the version is V6.0 SP1.1 or higher (like V6.0 SP2.0)
Vijeo Designer will work with Windows 7 32 bit also.
Note: You can NOT install V6.0 on a Windows 7 64 bit PC, as it’s only suitable for 32 bit machines, this means you actually install SP1.1 directly, as in reality this is a full version.
You then register the details of the new V6.0 CD, or V6.0 update CD serial number and part number.
Customers can download Vijeo Designer Service packs form the new eclipse site as long as they have an active subscription, and can be found under patches.
Was this helpful?
What can we do to improve the information ?