Technical FAQs

Ask a Question

Will GV2, GV3 and GV7 get de-rated with altitude? How will the de-rating work?


Yes, for altitudes higher than 2000 metres, see below the de-rating on this table:
 
Altitude
Ue
Ie
2000 m
1 (no de-rating)
1 (no de-rating)
2500 m
0,9
0,92
3000 m
0,8
0,90
3500 m
0,7
0,88
4000 m
0,6
0186
Was this helpful?
What can we do to improve the information ?