Technical FAQs

Ask a Question

Do sphere lighting controllers need a live and a neutral supply?

Sphere 5 and 8 Channel Hand and Wall Controllers are battery powered only, the various types of receivers are the only system components that are permanently connected to the mains wiring. Please refer to attached information for further details.
Was this helpful?
What can we do to improve the information ?