Technical FAQs

Ask a Question

What’s the heat dissipation on the LRD range of overloads?


Reference
Setting range
Power dissipated in
 
 
 VA at Ith max.
LRD01
0.1-0.16
1.33
LRD02
0.16-0.25
1.4
LRD03
0.25-0.40
1.38
LRD04
0.40-0.63
1.24
LRD05
0.63-1
1.55
LRD06
1-1.6
1.61
LRD07
1.6-2.5
1.67
LRD08
2.5-4
1.61
LRD10
4-6
2.14
LRD12
5.5-8
1.83
LRD14
7-10
1.77
LRD16
9-13
2.42
LRD21
12-18
1.99
LRD22
16-24
2.53
LRD32
23-32
2.43
LRD35
30-38
3.04
LRD3322
17-25
3.42
LRD3353
23-32
3.81
LRD3355
30-40
4.52
LRD3357
37-50
6
LRD3359
48-65
7.98
LRD3361
55-70
8.18
LRD3363
63-80
10.17
LRD3365
80-104
5.62
LRD4365
80-104
6.7
LRD4367
95-120
8.35
LRD4369
110-140
10.38
LRD33656
 80-104
7.57
LRD33676
95-120
9.5
LRD33696
110-140
11.95


Note: Power dissipated per pole
Was this helpful?
What can we do to improve the information ?