Technical FAQs

Ask a Question

Where can I locate information covering the LK3 (and LK31) switch disconnect products?

The LK3 switch disconnect products (suitable for load break and isolation applications in accordance with catalogue specifications) are marketed by Schneider Electric specifically in the UK.
As a result, information is not presented on the global web site.

The LK3 (also LK31 prefix on larger versions) covers ratings from 40A Ith through to 1250 Ith in 3 and 4 pole versions. 

Please note: Switch disconnect kits (part number LK3***0 or LK31***0) include the switch body that has the same part number as the kit but without the 0 (zero) suffix, e g kit LK3AT30 contains body LK3AT3.

Further information covering full product specifications and including separate component parts can be found by downloading the PDF catalogue attachment (see link below).

Was this helpful?
What can we do to improve the information ?