Technical FAQs

Ask a Question

Can I get the magnet or the detector of a Coded Magnetic Switch XCS for Safety, as separate component?

No, the Safety coded magnetic switches have to be bought as a pair, which will include the magnet and the detector.

Note: Other variations on the parts will also be added onto the part number of the pair, like a different cable length.
Example: XCSZP70010 is not sold separate, you can get: XCSDMP70010
XCSDMP70010 = XCSZP70010 + XCSZP1
Was this helpful?
What can we do to improve the information ?