Technical FAQs

Ask a Question

What replaced XPSCE? What are the differences between XPSCE and the new XPSCM?

XPS-CE Replaced by XPS-CM
XPSCE (old model)                                                       XPSCM (new model)

  • XPS-CM has 3 extra solid state outputs for PLC signalling
  • XPS-CM has choice between 2 models with or without removable plug terminals (P)
  • XPS-CM has muting lamp error detection
  • XPS-CM has only one muting lamp connection
  • XPS-CM uses 4 muting sensors

Schematic Comparisons
Monitoring of 4 XU2-S single beam detectors with muting function

Cross Reference Table
NOTE: Data sheets about new safety relays XPSCM are available on the website to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?