Technical FAQs

Ask a Question

What replaced XPSASF? What are the differences between XPSASF and the new XPSAK?

XPS-ASF Replaced by XPS-AK
XPSAFS (old model)                                                    XPSAK (new model)

  • XPS-AK has one extra N/O safety output
  • XPS-AK has one extra additional N/C output
  • XPS-AK has 2 extra solid state output for PLC signalling
  • XPS-AK has choice between 2 models with or without removable plug terminals (P)
  • XPS-ASF could’ve been used for Type III A two-hand control monitoring

Schematic Comparisons
Monitoring of E-stop with 2N/C contacts

Monitoring of safety mat with E-stop button


Cross Reference Table

NOTE: Data sheets about new safety relays XPSAK are available on the website to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?