Technical FAQs

Ask a Question

What replaced XPSAP? What are the differences between XPSAP and the new XPSAR?

XPS-AP Replaced by XPS-AR
 
XPSAP (old model)                                                                   XPSAR (new model)




  • XPS-AR has one extra N/O safety output
  • XPS-AR has one extra additional N/C output
  • XPS-AR has 4 solid state output for PLC signalling
  • XPS-AR has choice between 2 models with or without removable plug terminals (P)
  • XPS-AP could’ve been used for Type III A two-hand control monitoring

Schematic Comparisons
 

 
Monitoring of E-stop with 2N/C contacts
 
 


 
Monitoring of E-stop with 1N/C contacts 





Monitoring of E-stop with 2N/C contacts in series
 
 


 
Monitoring of a movable guard associated with 2 limit switches with 1 contact each





Cross Reference Table


NOTE: Data sheets about new safety relays XPSAR are available on the website to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?