Technical FAQs

Ask a Question

Can I connect an SR2 or SR3 Zelio Logic Smart Relay to an HMI, separate display screen?


Yes, you can connect the SR2 or SR3 to a small HMI, this HMI comes included in a kit, starter-kit HMISTO & Zelio Logic – reference: VJDSTKSTOSR2

 
The starter-kit HMISTO & Zelio Logic, reference VJDSTKSTOSR2, includes:
  • 1 Small Panel HMISTO501 (specific HMI to work with the Logic relays SR2 and SR3)
  • 1 Zelio Logic SR2B121BD (24VDC 12 I/O with clock)
  • 1 VijeoDesigner Demo on USB Key + leaflet to explain how to use the USB key
  • 1 Zelio Software SR2SFT01 + 1 USB download cable SR2USB01
  • 1 Link cable between HMISTO501 & Zelio SR2CBL09
  • 1 Power Supply ABL8MEM24012 1 phase 24VDC 1,2A




 HMISTO501 characteristics:
  • 3”4 monochrome screen with a 3-color backlight Green / Orange / Red.
  • 9-pin terminal block RS232C allowing the communication with Zelio Logic PLC and the new cable SR2CBL09.
  • 2 USB ports type mini-B device and type A host to allow easy application download via standard USB cable or USB keys
  • Support of USB peripherals: Code reader, Memory device, USB to Serial.
The quick mounting is always done tool-free with 2 spring clips                                       


NOTE: A data sheet about this kit is available on the website to download, use the search engine (top right corner) reference SE7413. Documentation of the individual documentation available.
Was this helpful?
What can we do to improve the information ?