Technical FAQs

Ask a Question

What replaced XPSAPF? What are the differences between XPSAPF and the new XPSAR?

XPS-APF replaced by XPS-AR

 XPSAPF (old model)                                                    XPSAR (new model)


  • XPS-AR has 2 extra solid state outputs for PLC signalling
  • XPS-AR has choice between 2 models with or without removable plug terminals (P)
  • XPS-AR has 1 extra N/O safety outputs
  • XPS-AR cannot monitor safety mats or edges
  • XPS-APS could be used for Type III A two-hand monitoring

Schematic Comparisons

Monitoring of E-stop with 2N/C contacts
 


Cross Reference Table


NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
 
See also FAQ number FA141626
Was this helpful?
What can we do to improve the information ?