Technical FAQs

Ask a Question

What replaced XPSAM? What are the differences between XPSAM and the new XPSAK?

XPS-AM Replaced by XPS-AK

 XPSAM (old model)                                                            XPSAK (new model)

  • XPS-AK has choice of removable plug terminals
  • XPS-AK has 45mm width
  • XPS-AK has 4 solid state output for PLC signalling
  • XPS-AM could be used for Type III A two-hand control monitoring
  • Check also FAQ number FA140665

Schematic Comparisons
Monitoring of E-stop with 2N/C contacts

Monitoring of E-stop with 1N/C contact

Monitoring of E-stops with 2N/C contacts in series

Monitoring of a movable guard associated with 2 limit switches with 1 contact each


Cross Reference Table

NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?