Technical FAQs

Ask a Question

What replaced XPSAM? What are the differences between XPSAM and the new XPSAF?

XPS-AM Replaced by XPS-AF

 XPSAM (old model)                                                     XPSAF (new model)

  • XPS-AM has 1 extra additional N/C output
  • XPS-AF has 22.5mm width
  • XPS-AM had larger range of supply voltage selection
  • XPS-AM could be used for Type III A two-hand control monitoring
  • XPS-AF has choice of removable plug terminals (P)
  • Check also FAQ number FA140672
Schematic Comparisons
Monitoring of E-stop with 2N/C contacts

Monitoring of E-stop with 1N/C contact

Monitoring of E-stops with 2N/C contacts in series

Monitoring of a movable guard associated with 2 limit switches with 1 contact each

Cross Reference Table

NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)

Was this helpful?
What can we do to improve the information ?