Technical FAQs

Ask a Question

What replaced XPSAMF? What are the differences between XPSAMF and the new XPSAK?

XPS-AMF Replaced by XPS-AK
 
  • XPSAMF (old model)                                                   XPSAK (new model)



  • XPS-AK has 2 extra solid state output for PLC signaling
  • XPS-AMF can be used for Type III A two-hand control monitoring
  • XPS-AK has choice between 2 models with or without removable plug terminals (P)
Schematic Comparisons
 
Monitoring of E-stop with 2N/C contacts



Monitoring of safety mat with E-stop button




Cross Reference Table


NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?