Technical FAQs

Ask a Question

What replaced XPSAS? What are the differences between XPSAS and the new XPSAF?

XPS-AS Replaced by XPS-AF
XPSAS (old model)                                             XPSAF (new model)

  • XPS-AF has one extra N/O safety output
  • XPS-AF is 22.5 mm width
  • XPS-AS has larger range of voltage selection
  • XPS-AS can be used for Type III A two-hand control monitoring
  • XPS-AF has choice between 2 models with or without removable plug terminals (P)

    Schematic Comparisons
    Monitoring of E-stop with 2N/C contacts

    Monitoring of E-stop with 1N/C contact

    Monitoring of E-stops with 2N/C contacts in series

    Monitoring of a movable guard associated with 2 limit switches with 1 contact each

    Cross Reference Table

    NOTE: Data sheets about new safety relays XPSAF are available on the web site to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?