Technical FAQs

Ask a Question

Can the switching half of a coded magnetic switch be bought by itself without the magnet half?

No. Although the switched half of the coded magnetic switch often has a number printed on it, it cannot purchased separately. The switch has to be purchased with the magnet as a complete switch pair. E.g. the coded magnetic switch XCSDMP7002 has the number XCSZP7002 printed on the switched half of the switch pair, however the XCSZP7002 cannot be purchased separately. If the switched part (XCSZP7002) is required then the complete  XCSDMP7002 has to be purchased.
Was this helpful?
What can we do to improve the information ?