Technical FAQs

Ask a Question

What replaced XPSAX? What are the differences between XPSAX and the new XPSAC?

XPS-AX Replaced by XPS-AC
XPSAX (old model)                                                      XPSAC (new model)

  • XPS-AC has a solid state output for PLC signaling
  • XPS-AX has one additional N/C output
  • XPS-AC has larger range of supply voltage selection
  • XPS-AC has choice between 2 models with or without removable plug terminals (P)

    Schematic Comparisons
    Monitoring of E-stop with 2N/C contacts


           Monitoring of E-stop with 1N/C contact


Cross Reference Table

NOTE: Data sheets about new safety relays XPSAC are available on the web site to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?