Technical FAQs

Ask a Question

What replaced XPSAL? What are the differences between XPSAL and the new XPSAC?


XPS-AL Replaced by XPS-AC

XPSAL (old model)                                                      XPSAC (new model)



  •        XPS-AC has one extra N/O safety output
  •        XPS-AC has a solid state output for PLC signaling
  •        XPS-AC has choice between 2 models with or without removable plug terminals (P)



Schematic Comparisons

Monitoring of E-stop with 2N/C contacts



Monitoring of E-stop with 1N/C contact



Cross Reference Table



NOTE: Data sheets about new safety relays XPSAC are available on the web site to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?