Technical FAQs

Ask a Question

What is the part number for the blank marker legends for the Modular GC or CT2000 range of contactors?

The part number is LA9D90. It is a clip on front mounted 8 X 17mm white plastic legend. These are also used on the TeSys K contactor range.

Was this helpful?
What can we do to improve the information ?