Technical FAQs

Ask a Question

What replaced XPSAS? What are the differences between XPSAS and the new XPSAK?

XPS-AS Replaced by XPS-AK

XPSAS (old model)                                                      XPSAK (new model)

  • XPS-AK has 1 extra N/O safety output
  • XPS-AK has 1 additional N/C output
  • XPS-AK has 4 solid state output for PLC signaling
  • XPS-AK has choice between 2 models with or without removable plug terminals (P)
Schematic Comparisons
Monitoring of E-stop with 2N/C contacts

Monitoring of E-stop with 1N/C contact

Monitoring of E-stops with 2N/C contacts in series

Monitoring of a movable guard associated with 2 limit switches with 1 contact each

Cross Reference Table

NOTE: Data sheets about new safety relays XPSAK are available on the web site to download, use the search engine (top right corner)
Was this helpful?
What can we do to improve the information ?