Technical FAQs

Ask a Question

Can the class 20 LRD15.. thermal overloads be used with LC1D38.. contactors?

Although the LRD15.. overload setting range only goes up to 32 amps you can fit any one of these overloads to an LC1D38.. contactor.
The LC1D38.. contactor shares the same frame body as the LC1D25.. and the LC1D32.. contactors.
Was this helpful?
What can we do to improve the information ?