Technical FAQs

Ask a Question

How do I work out what a 9012G or 9016G range pressure switch is from the part number

The part number for a 9012G and 9016G is made up from the following table

Electrical Connections : 1/2”-14 NPTF, PG13.5, or ISO M20. For metric threads, add M after the W on all types. eg 9012GAWM1

Also the following variants may exist

Was this helpful?
What can we do to improve the information ?