Technical FAQs

Ask a Question

Can I change prices in Spacial.pro?

Yes you can change prices. You can also change discounts.
Price files are in Excel format and are located in …\My Documents\Schneider Electric\Spacial.pro v****\Prices.

 There are two Pricing Files, one for the Enclosures and one for Devices as shown below
Spacil Pro showing the two Price files Devices and Enclosures
These files have an Excel tab for "Public Price" which is the List Price for each item
Spacial Pro excel file showing the Public or List pricing for each item
They also have an Excel tab marked "Discount" which contains the "Standard Discount" and Exceptional Discount" for each product.
Spacial Pro showing the Excel file with the Discount tab for Standard and Exceptional Discount percentage per Item

Was this helpful?
What can we do to improve the information ?