Technical FAQs

Ask a Question

Can I change the save directory in Spacial.pro?

Yes, you can select a different target directory, see below
Warning : When you restart, Spacial.pro reopens with the default directories.

There are two ways to change the directory

  • Using the bottom tool bar "Save As" option as shown below, then changing the path for the file
Using the "Save As" function in Spacial Pro to alter the location for the saved project
  • Using the "Save Current Project" function in the "Home" tab and then changing the path for the file
  •  Using the Save Current Project function in Spacial Pro to change the path for the saved file
Was this helpful?
What can we do to improve the information ?