Technical FAQs

Ask a Question

Where can I find information covering the LE1GB, LE2GB or LE3GB enclosed DOL, reversing and star delta starters?

The LE1GB, LE2GB or LE3GB enclosed DOL, reversing and star delta starters are only marketed in the UK
They appear on Schneider Electric web site searches under the following path
Home > Products and Services > Automation and Control > Product offers > Motor Control > Enclosed motor starters > LE*GBT

Unfortunately the current search system will not locate them as they are a local UK offer

This range of enclosed starters are IP65, have a robust metal base and a polycarbonate cover.
Versions are available with or without a disconnect switch.

Information covering these products is provided as a PDF attachment (see bottom of page) for reference.

Important notes:

These starters are supplied without thermal overload relays fitted.
Separate overloads should be selected as follows based on the motor full load current (FLC) or in the case of the star delta starters the FLC x 0.58.

Starters LE*GBK use LR2K* thermal overload relays, starters LE*GBT use LRD* thermal overload relays as detailed below;






Was this helpful?
What can we do to improve the information ?