Technical FAQs

Ask a Question

What are the recomendations when installing the Sphere Wireless Lighting System in an Outdoor Lighting Application?

All outdoor garden installations must be installed in accordance with IEE Regulations for Special Installation Requirements. A 30mA RCD (Residual Current Device) should always be placed between indoor and outdoor electrical circuits, including the initial connection to an outdoor transformer used for Low Voltage lighting. 

Note that the Floor and Ceiling Receivers do not have enhanced IP ratings. They should be either wired such that they are located indoors or, if required to be located outdoors, housed in a suitable weatherproof enclosure of at least IP56 rating. Outdoor enclosures must be constructed and located such that the Sphere receivers cannot overheat – for example, not in direct sunlight
Was this helpful?
What can we do to improve the information ?