Technical FAQs

Ask a Question

Can I have more than one Sphere Wireless Lighting Controller in a room?

 
Multiple Controllers can be used to control the same lights in a room (e.g. 1 Wall Controller and 1 Handheld Controller). Controllers are added by simply duplicating the House, Room and Mode switch settings on each of the additional Controllers.

Note if a Controller sends the same command as the previous command sent from another Controller, there will be no response. A second button push will be required. (This is a result of the last Controller command information being held only in the Receivers).
 
One Controller can dim the channels and an alternate Controller can operate scenes. To do this set the dimming/scene switch to ‘D’ or ‘SC’ as required
Was this helpful?
What can we do to improve the information ?