Technical FAQs

Ask a Question

What is happening if the Sphere Wireless Lighting System seems to change by itself?

Sphere control commands are heavily encrypted. As such unexpected changes to the lighting in one or more rooms can only be caused by Sphere Controllers that have the same switch settings being operated nearby, for instance in adjacent rooms or neighbouring apartments that have the Sphere system. However it is still possible that interference could occur if a new Sphere system is installed locally. In this case, the House switch settings on the Controller of the affected room(s) will need altering.

Was this helpful?
What can we do to improve the information ?