Technical FAQs

Ask a Question

How do I replace a lost or damaged Sphere Controller?

 
If a Controller is damaged or lost, obtain a replacement and find the record made of the switch settings on the old Controller then duplicate these exactly on the new Controller. Since all the channel and scene settings are stored in the Receivers, no reprogramming is necessary
Was this helpful?
What can we do to improve the information ?