Technical FAQs

Ask a Question

Are the Exclusive white moulded RCD sockets Latching or Non Latching?

The LSKT1GR & LSKT2GR are non latching (Active). If the power is removed the socket will trip and need to be reset once power is restored. The device will fail safe in the event of loss of supply.

The LSKT2GRP are latching (Passive) and will only trip in the event of a fault. These are suitable for freezers and commercial applications
Was this helpful?
What can we do to improve the information ?