Technical FAQs

Ask a Question

Can I modify Price files and User Catalog file outside Spacial.pro?

Yes. Price files will be loaded again during the next start of Spacial.pro.
If the application is already open during the work on these files, you just have to click on "Update" button, located in the bottom tool bar.
This allows you to Load the Prices, Refresh the Prices or Refresh the User Catalogue as shown below.

How to Load the Prices, refresh thePrices or the User Catlaogue in Spacial Pro

If "Loading Prices" is selected then the location of the new Pricing Zip file is requested
Selecting "Refresh Prices" re-imports the Price file, thus updating any changed information from the excel file
Selecting "Refresh User Catalogue" re-imports the User Catalogue, thus updating any changed information from the excel file
Warning: If the User Catalogue excel file is modified, Clicking on the "Update" button is mandatory to update "User Catalog".
              If the Pricing excel file is modified, Clicking on the "Update" button is mandatory to update "Pricing".

 The other method of updating the User Catalogue or Pricing files is via the Settings Menu as shown below

How to update the user catalogue in Spacial Pro via the settings menu

Was this helpful?
What can we do to improve the information ?