Technical FAQs

Ask a Question

Where is located Spacial.pro User Catalog source file?

During the installation, Spacial.pro creates a directory named “UserCatalog” and located in My Documents\Schneider Electric\Spacial.pro v*****
The work file is called: UserCatalog.xls. It must not be moved.
File location of Spacial Pro User Catalogue

The if the file is modified you need to load the changes by importing the file, this is done in the setting function
Click on the settings icon, located in the bottom bar and the click on "Edit End User Catalogue" as shown below
The excel file contains all the instructions on haw to modify the file.
How to Import or update the End User Catalogue in Spacial Pro

Was this helpful?
What can we do to improve the information ?