Technical FAQs

Ask a Question

In Spacial.pro, why does the language not change immediately after the parameter has been modified?

The interface is initialized during the application’s launch. Change the language then restart the software.

To change the Language, open the settings functions from the icon in the bottom bar.
As shown below you can select the Language from the drop down which will show the loaded Languages.
Changing the Language in Spacial Pro

Was this helpful?
What can we do to improve the information ?