Technical FAQs

Ask a Question

In Spacial.pro, can I add products from “Other Accessories” in the “Graphical Design” window?

No. There are two reasons why a component is located in “Other Accessories” tab:

1. This component does not define the dimensions of the equipment

2. This component does not have yet the mandatory characteristics to be displayed: no dimension or no CAD drawing.

In the second case, future updates of the database will progressively improve this information.
Was this helpful?
What can we do to improve the information ?