Technical FAQs

Ask a Question

What is the difference between “External Product” and “User Catalog” folders installed by Spacial.pro?

 External Product: contains examples of Excel files allowing you to enter a list of products (graphical or not, known by the database or not) coming from an external source. The main goal is to accelerate the selection of components in Spacial.pro.

The External Project file can be loaded in to an open project as shown in the screen shot below
Location of External Products file in Spacial Pro
The External Project file is an Excel file that can be edited as shown below
View of contents of the External Products file in Spacial Pro

The screen shot below shows how the Components in the External File are displayed in a Spacial.Pro project once loaded
View of how the External Products are displayed when loaded in to a Project

User Catalogue: contains the Excel file that manages the product list of a local catalog that the user can entirely manage himself: reference codes, nodes hierarchy, pictures and CAD drawings.

The screen shot below shows how to access the End User Catalogue in Spacial Pro
Once opened the Excel File contains detailed instructions, in the first tab, on how to modify the file.
Location of the User Catalogue in Spacial Pro
Was this helpful?
What can we do to improve the information ?