Technical FAQs

Ask a Question

Can I import a CAD Drawing in Spacial.pro?

Yes. It is possible to import DWG drawings thanks to User Catalog.
Setting and Editing "User Catalogue"
Click on the Settings Icon as shown above
Then Edit the "User Catalogue" and follow the instructions in the excel file that opens.

Note: It is not possible to import a complete “Equipment” after having exported it.

Was this helpful?
What can we do to improve the information ?