Technical FAQs

Ask a Question

Can I display the scale horizontally in Spacial.pro?

The scale can only be displayed vertically.
Spacial.Pro scale on drawing

To take horizontal measures, use the dimension tool.
This is shown in the Right Hand tool bar as shown below.
To measure, click on the icon then on the two points that you wish to measure between.
Measure distance in Spacial.Pro

Was this helpful?
What can we do to improve the information ?