Technical FAQs

Ask a Question

What is the meaning of the blue square in Spacial.pro?

The blue square is a magnetization point that appears when two components are close.
It allows you to align two products. An example is shown in the image below
Spacial.pro showing the blue square that indicates a snap or magetization point

Was this helpful?
What can we do to improve the information ?