Technical FAQs

Ask a Question

When I double-click in Spacial.pro on some components, they do not appear in the graphical area. Why?

In Spacial.pro v1.0, double-click is possible on all components, excepted in User Catalog.
Indeed, an alert message indicating that the action is impossible will appear on bottom left of the tab, as shown in the screen shot below
Screen Capture showing the error if a component from the User Catalogue is double clicked

Was this helpful?
What can we do to improve the information ?