Technical FAQs

Ask a Question

In Spacial.pro, how can I move components?

Click on the features of the drawing representing the component to select the component, the component selected will change to a dotted line style (see image below).
Click and move the component with your mouse, this will be the locus (fixing point) of the movement.
Each component has a fixing point or origin, show by a red square (see below)

Image showing the Origine point, a red square, for a component in Spacial Pro

If you select the component near the origin point you will see the origin changes from a red square to a green square. This indicates that you have picked the component by its origin.
Finally click again in the new location to fix the component in place.

Was this helpful?
What can we do to improve the information ?