Technical FAQs

Ask a Question

Can I add more poles to a DF fuse carrier

Yes, Additional power poles and neutral links and auxiliaries can be added
To do this fuse carrier assembly kits are used as detailed below

Fuse carriers  
to be
Size of cartridge
fuse or link
Composition Unit
DF8 8.5 x 31.5 1 pin, 2 clips DF10AP
DF10 10 x 38 1 pin, 2 clips DF10AP
DF14 14 x 51 1 pin, 3 clips DF14AP
DF22 22 x 58 1 pin, 3 clips DF22AP

Was this helpful?
What can we do to improve the information ?