Technical FAQs

Ask a Question

What communications profiles are available on the XPSMF Preventa Safety PLC's

There are several communication protocols available for the XPSMF safety PLC's they are detailed below

  • Safe Ethernet
  • Modbus TCP/IP server protocol
  • Modbus Serial (RTU)
  • ProfiBus DP
A chart showing the compatibility in more detail is below

Was this helpful?
What can we do to improve the information ?