Technical FAQs

Ask a Question

How can I test an LT47 is functioning

To test if an LT47 is functioning at No Load follow the procedure below

When LT47 is powered,
keep Test button pushed for

  • D-Time plus O-Time (Manual reset type)


  • O-Time (Auto reset type)
The internal relay switches its contact.

Periodic test is recommended.

Was this helpful?
What can we do to improve the information ?