Technical FAQs

Ask a Question

Can I remotely reset the LT47 electronic overload relay

The LT47 Electronic Overload is available in two formats

LT47***S - With Manual or Electric Reset
LT47***A - with Automatic Reset

Electric reset is only available in the LT47***S
To perform an Electric Reset : Interrupting control power (minimum 0.1s).

Was this helpful?
What can we do to improve the information ?