Technical FAQs

Ask a Question

What is the maximum number of units that can be stacked on an XVE Beacon

It is possible to stack up to five units on the XVE beacon base
  • 4 Illuminated units and 1 audible unit
  • 5 Illuminated units

Was this helpful?
What can we do to improve the information ?